Harmonic Drive aboutusHarmonic Drive ProductsHarmonic Drive ReferenceHarmonic Drive SupportHarmonic Drive Sales ContactsHarmonic Drive Employment Opportunities
PAGE: "Reference | Application Notes | Installation Considerations for Gearheads :: Harmonic Drive LLC"
URL: http://legacy.harmonicdrive.net/reference/applicationnotes/installgh.php

Application Notes



Installation Considerations for Gearheads

The following information is directed toward technicians or personnel, who are involved in the assembly or installation of Harmonic DriveĀ® strain wave gearing.
  1. Refer to the motor mounting tolerances and gearhead drawing for proper installation specifications.
  2. Wave Generator must be securely fastened to the input hub to prevent axial movement along the input shaft.
  3. Wave Generator must be assembled concentrically with the Circular Spline to prevent an improper assembly. Refer to the section named "Dedoidal" in our catalog.
  4. Proper seals, gaskets, or sealants must be used to contain the small amount of oil that may separate from the grease.
  5. Only the specific Wave Generator supplied with each gearhead may be used with that gearhead. These are shipped as a matched set.
  6. The input/output shaft of this unit has been coated with a rust preventative wax for storage purposes, and must be thoroughly cleaned with ethyl or methyl alcohol prior to use. To avoid deterioration of the oil seal, do not use acetone, thinner, or gasoline.

We encourage you to call us at 800-921-3332 or 978-532-1800 if you have any questions or comments.




[ Harmonic Drive LLC | About Us | Products | Reference | Support | Disclaimer ]
© 2026 Harmonic Drive LLC | 800-921-3332
The leader in high precision motion control.
Harmonic Drive is a registered trademark of Harmonic Drive LLC.
Long Island Web Design